Part Number: LSF0108
Hi team,
Our customer is using this LSF0108 for quad SPI which means it has bidirectional signal.
Customer wants to transfer from 1.8V to 3.3V.
1. May I know which signal to pull up? only 3 signal need to be pulled up?
2. Pull up on which side?
3. Does the pull up resistor the same on both side? According to table5. For 15mA, does this mean to 97ohm and 197ohm on each side?