This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC08A: 50MHz clock buffer for ADS8920B SCLK input

Genius 16605 points
Part Number: SN74LVC08A
Other Parts Discussed in Thread: ADS8920B, , SN74LVC1G17, SN74LVC1G34

Hello,

Our customer is considering to use SN74LVC08A as a buffer to 50MHz SCLK input of ADS8920B.
Can SN74LVC08A be used for this purpose? 
ADS8920B SCLK reqruies 45-55% high/low time clock with VIH= 0.7 VCC / VIL=0.3VCC (VCC=3.3).

Regards,
Oba