Other Parts Discussed in Thread: SN74AXC8T245
Hi,
Customer uses LSF0108 with below schematic, the input signal from P1V8 side(directly connected to the transmission chip without pull-up resistor) is output to P3V3 end via LSF0108( P3V3 side using 220ohm resistor), and found a low level voltage 600mV; LSF0108 output signal is very poor when connecting to the terminal device(only 0ohm string resistance from SF0108 to terminal device); the signal has not significantly improved when trying to shorten the LSF0108 to the terminal chip distance; the signal is almost normal, except the 600mV low level offset when removing the terminal device.
Could you help to check what would cause this kind issue? How to improve the signal performance?
schematic:
test waveform:
1. pull up resistor in RXD0 side is 220ohm
before level-shift(1.8V terminal )
after level shift(3.3V terminal), the high level is not rising to 3.3V.
removing the terminal device at 3.3V side.
Thanks.