This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Schmitt trigger input with 5v to 3.3v level shift

Other Parts Discussed in Thread: SN74LVC1G17

Hi,

I'm looking for a single bit Schmitt trigger  input device.

Inverter or buffer will work

Input signal is a pulse up to 2 megahertz open drain with a 220 ohm pull-up resistor to 5 volts

Output required is a clean 3.3 volt  pulse to drive the input of an fpga.

Many years ago I used a 74hc14 plus sn74cbt3384 but I would like to update to a single chip single channel solution.

Thank you,

Wayne