Part Number: SN74HCT04
Are below target device support wave soldering?
・SN74HC04DR
・SN74AS1034ADR
・SN74ALS1034DR
・The other 14pin SOIC standard logic's
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes. See, for example, these application reports:
Wave Solder Exposure of SMT Packages
Solder Pad Recommendations for Surface-Mount Devices
Recommended Soldering Profiles
Mounting of Surface Mount Components