This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G125: SN74LVC2G125

Part Number: SN74LVC2G125


About SN74LVC2G125 datasheet,

6.3 Recommended Operating Conditions,

IOH (High-level output current), VCC = 3 V, what is the different condition between -16mA and -24mA?

IOL (Low-level output current), VCC = 3 V, what is the different condition between 16mA and 24mA?