This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC24T245: 24MHz 16ch 1.8 to 3.3V logic

Part Number: SN74AVC24T245


Hi,
I need to translate from 1.8V to 3.3V of the logic signals (16 signals in total) whose max frequency is 24MHz.
In addition, the space on the PCB is really small.

Keeping in mind that the BGA solution is certainly the most compact and that I would not want to spend a lot for a translator .... I have identified:

SN74AVC24T245 (e.g. SN74AVC24T245ZRGR).

Unfortunately the 16ch gives it to me in end of life ... so I selected the 24ch.
What I ask you is:
1. To support me in choosing the best component to which you want to direct me, do you have anything else that can work well at these frequencies, reasonable cost and with limited dimensions?
2. To help me understand if the SN74AVC24T245ZRGR is indicated for the application since, unfortunately, in the DS I have not found the Tw parameter (or equivalently Tsu and Th) to verify that the max freq is supported. In tests there is a 10MHz test signal .... but I would not like to risk that the bandwidth is insufficient.

Many Thanks,

Antonio