Part Number: CD4027B
Other Parts Discussed in Thread: CD4016B, , TS12A4514, CD4066B
Dear * all,
i changed the input buffer form CD4050B for a CD40106B so i connected
-> button from Pin1 ( CD4016B) to gnd, and added a 100k pull-up to 12V from Pin1 ( CD4016B)
-> when i press the button Pin2( CD4016B) goes UP ( this works ok)
-> then i connected J2 and K2 from CD4027BE to 12V, Set2 and Reset2 to GND .
-> and finaly i connected the PIN2 (CD4016B) direct to PIN3 (CD4027BE)
and now the Q2 and !Q2 stay after input change in they state.
But sometimes after button press the output Q won't change?
1) do i need an RC IN pin1 of CD4016B?
2) do i need a pull-down on pin3 CD4027B?
3) do i need a RC on pin3 CD4027B?
[ i currently don't have access to a scope ]
Best Regards.