This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC1T45: SN74AVC1T45

Part Number: SN74AVC1T45


Hi,

I want to understand if this chip can handle a frequency of 40MHz LVCMOS clock on its input?

The datarate says 500MBPS so i am assuming the frequency it can handle is nearly 500MHz for 1.8V to 3.3V.

Is this correct? the datasheet talks about 10MHz frequency only.

thank you for the reply.

thanks

Prasanthi