Other Parts Discussed in Thread: 14-24-LOGIC-EVM
Hi team,
Good day.
Our customer would like to use the SNJ54LS266W, however, due to the long lead time they are looking for an alternative. It seems that the SNJ54LS266W is the only XNOR device in CFP package. Thus, as an option, they're looking into the SN54LS266J and SNJ54LS266J. These devices are in CDIP package and based on the datasheet, it seems that part in CDIP and CFP package have the same pinout.
Is there a socket or breakout board that would allow for the installation of the CDIP packaged part into the CFP footprint?
Regards,
Carlo