This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV1T126: Level shifter understading differences between components

Part Number: SN74LV1T126

Hi:

I´m interested to aply a level shifter to a rgb adressable strip control, it has the next atributes and i want to understand better the component to use:

-VCC of 5 Volts

-Vin (data input) 0.7VCC (3.5V minimum ti have high state), less than 

-GND

My micro controller only has 3.3V outputs so i need domething to leveling up to >3.5V, i have the next components checked for that purpose:

-SN74LV1T126

-LSF0204

-Others?

Thank you.