Part Number: SN74LVTH32245
Other Parts Discussed in Thread: SN74LVTH16245A, SN74LVTH162245, SN74LVTH573, SN74LVTH16373
Hello Team,
My customer has been using the the following devices in several projects.
- SN74LVTH32245ZKER
- SN74LVTH32373ZKER
The possible alternatives were,
Alternatives for SN74LVTH32245ZKER:
- SN74LVTH16245A DGVR , no 1:1 replacement, DGV-TVSOP48-Package
- SN74LVTH162245 DGGR , no 1:1 replacement, DGG-TSSOP48-Package
- SN74LVTH16245A DLx , no 1:1 replacement, SSOP48-Package
Alternatives for SN74LVTH32373ZKER:
- SN74LVCH32373A ZKER , which seams to be a 1:1 replacement for me at 3.3V Vcc; => Is this component still available after Jan 7, 2021? I did not find it in the PDN !
- SN74LVTH573 RGYR , no 1:1 replacement, VQFN20-Package
- SN74LVTH16373 DGGR ,no 1:1 replacement, TSSOP48-Package
Questions:
- Do we have any other suggestions for replacement parts?
would prefer 1:1 replacement with long term availability.
- What are the status of the replacement components mentioned above?
Which of them should I use for long term availability and which of them
can get or are planed to get a PDN in the near future?
Thanks in advance.
Best Regards,
Needhu