Part Number: SN74AXC8T245EVM
Hello team,
My customer purchased the SN74AXC8T245EVM and performed a quick test.
- Supplied VccA = 1.8V and VccB = 3.3V from a bench-top power supply.
- Fed A1 (SMB connector) with a 125MHz clock from an Agilent 81130A pattern generator at 1.8V and observed B1 (SMB connector) on a scope.
- Customer noticed that when they turned on the output of the pattern generator, the VccA rail would rise from 1.8V to about 2.34V, and the output high level would be around 2.0V.
Do you have any suggestions on why the VccA rail is rising and the output level of the B channel is not at the 3.3V? Lowering the frequency of the input signal did not seem to have any effect on the outcome.
Thank you for your support!
Errol