Part Number: LSF0204
Dear Team,
Can LSF0204RUTR implement in MDC/MDIO 1.2V/1.8V transfer?
It seems ok:
But it also mentioned:
Or you have a better solution here?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LSF0204
Dear Team,
Can LSF0204RUTR implement in MDC/MDIO 1.2V/1.8V transfer?
It seems ok:
But it also mentioned:
Or you have a better solution here?
BR
Kevin
Dear Ladisch
Thanks for the comments.
I just want to double-check with you.
The datasheet suggests Vref_B have 1V higher than Vref_A for better signal integrity.
So if my customer wants to use it for 1.2V to 1.8V will be fine, it just doesn't have the best signal performance, right?
BR
Kevin
Hey Kevin,
The point Clemens was trying to make is that you don't need to have 1.8 V on VrefB, but instead have a higher voltage like 3.3 V to meet the recommended min spec. You can still pull the output up to 1.2 V.