Other Parts Discussed in Thread: SN54AHC541, SN54AHCT541
We are using a SN54ABT541BPWRE4 as a 5V device and have discovered that the Voh is rather low (3v min). We are seeing about 3.6V when we load with around 100K resistor. The output is too low for comfort. Are there any parts available that have a higher Vol (with 5Vcc). I’m looking for something with a Vol min of 3.5v when powered by 5v. The kicker is it has to have all of the same features and be a drop in replacement. Let me know if there is anything available.
I've seen the SN54AHC541 but the key feature that we are looking for is high impedance state during power up and power down. If the datasheet doesn’t specifically call out power up/down behavior, it may be a tough sell.