Part Number: LSF0204
Hi,
I am using LSF0204 for SPI communication lines. I am connecting Vref_B to 3.3V power source which is always supplying 3.3V to Vref_B without any control to turn it off.
Then I tie the EN pin toghether with Vref_A pin (1.8V), the EN pin will be HIGH and allow data transfer via the shifter whenever Vref_A pin receives input voltage. Am I right?
I know that when EN is LOW, level shifter will be in High-impedance state.
In my case, my concern is:
1. During High-impedance state, Vref_A willl be 0V and EN is LOW since they are tied. Therefore, does the level shifter still consume power due to the 3.3V power supply on Vref_B?
2. If the shifter still consumes power, how much power is being consumed due to Vref_B 3.3V supply voltage?
Please advise.
Thanks.