Hi team,
My customer now uses LSF0204, and pull up to 3.3V and 1.2V, pull-up resistor tries 330Ω and 1kΩ, but Vol of 1.2V side is always 350mV.
Can we make LSF0204 Vol drop to below 100mV? I don't think it's caused by their low input voltage, it seems caused by internal transistor.
If it's caused by internal transistor, do we have lower Vol device with same package and same data rate to promote? Or do we have solution to fix this?
Thank you!
Gary