Other Parts Discussed in Thread: SN74AXC2T245, SN74AXC4T245, SN74AVC2T245
Hi team,
I have a couple questions regarding TXS0102. First, can this device be used in situations where both VCCA and VCCB are 3.3V? The datasheet states that VCCA must be less than or equal to VCCB. Having VCCA = VCCB = 3.3V doesn't violate that or the Recommended Maximum Voltage of 3.6V on VCCA. I'm inclined to believe this is OK but I wanted to check.
Second, if VCCA is left floating for an extended period of time while VCCB = 3.3V, will this damage the device? I know you can leave the data pins floating, but I don’t see anything in the datasheet or on e2e that is conclusive one way or another about leaving VCCA floating.I know the device will not function, but will it be damaged?
Thanks,
Brian