This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1GX04: 27.12 MHz - queries

Part Number: SN74LVC1GX04


Hi Team,

My customer is planning to use SN74LVC1GX04 to generate 27.12 MHz frequency and have queries as listed below.

  1. Whether this device will support 27.12 MHz ? In the datasheet 27.12 MHz is not mentioned directly.
  2. We are planning to use crystal with load capacitance 10 pF and planning to use below values for external components ? CLOAD and RLOAD values. RF = 2.2 Mega Ohm, RS = 1 Kilo Ohm, CLOAD = ?, RLOAD = ?, C1 = C2 = 20 pF.
  3. From this device is it possible to take two,  27.12 MHz outputs to drive two devices. From 6th pin and 4th pin.

Please help with your comments and inputs.

Regards, Shinu Mathew.