Part Number: SN74LVC1G08
What is the exact input impedance value or range for SN74LVC1G08?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G08
What is the exact input impedance value or range for SN74LVC1G08?
The lowest input impedance can be derived from the worst-case input leakage current: 5 V / 5 µA = 1 MΩ. The typical leakage current is many orders of magnitude smaller, and is approximately zero at room temperature, so the upper limit of the input impedance is approximately infinite.
Hey Joe,
It can be anywhere from 10 to 25 ohms depending on the supply voltage.
Edit: Sorry I misread input for output, refer to Clemens' response on the input impedance.