Part Number: LSF0102
Hi Expert:
I have a design question that I want to confirm it with you.
Customer use a level shift IC (LSF0102) between BMC and LAN PHY (RTL8211F) for the management interface.
Q1: The level shift IC datasheet shows it needs pull-up resistors on A-side for both MDIO and MDC pins. Can you confirm it?
Q2: The datasheet said that No pull-up resistor is needed on the host side (3.3 V) if the LSF family is being driven by standard CMOS totem pole output driver.
If our BMC MDC pin is an output pin with CMOS type, does it mean we do not need add a pull-up on BMC side (B side of LSF0102)?
Regards,
Mark