Other Parts Discussed in Thread: CD74HC4046A, CD4046B,
Hi,
I would like to change 4MHz to 12MHz at Vcc=3.3V.
How should I choose external components?
Do you have any application notes?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to change 4MHz to 12MHz at Vcc=3.3V.
How should I choose external components?
Do you have any application notes?
Best Regards,
Kuramochi
Hello Kuramochi-san,
The SN74LV4046A is a direct replacement for the CD74HC4046A or CD4046B. There are two great application notes on using those devices that directly translate to the SN74LV4046A:
CMOS Phase-Locked-Loop Applications Using the CD54/74HC/HCT4046A and CD54/74HC/HCT7046A
Implementation of FSK Modulation and Demodulation using CD74HC4046A
You can also refer to the detailed information in the CD4046B and CD74HC4046A datasheets.
Please let me know if I can be of further assistance.