I am using the LS1012A,
which is a 1.8V processor, and I want to connect the external interface to 3.3V.
So, I want to use SN74AXC4T774-Q1, but there is no GPIO in the application of TI homepage.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using the LS1012A,
which is a 1.8V processor, and I want to connect the external interface to 3.3V.
So, I want to use SN74AXC4T774-Q1, but there is no GPIO in the application of TI homepage.
All devices can be used with GPIO. The SN74AXC4T774-Q1 works with LS1012A signals.
The 1T45 lists GPIO just because there is no other common application that uses a single channel, and leaving the application column empty would look bad.