Part Number: LSF0102
Hi,
LSF0102:
If one of the input voltage A or A and B is down and the EN pin is pull up, is the I/Os are in high Z state?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LSF0102
Hi,
LSF0102:
If one of the input voltage A or A and B is down and the EN pin is pull up, is the I/Os are in high Z state?
Hey Shay,
Are you referring to the supply pins being "down"?
The LSF has no power-down mode. As long as a current can flow into Vref_B and out of Vref_A (which can happen if Vref_A = 0), it might work.
The only way to disconnect the A and B side I/Os is to pull the EN pin low. (In most circuits, EN = Vref_B.)