This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0106: Alternate buffer for TXB0106 Level translator

Part Number: TXB0106


Hi,

   In our design, we are using 48 inch samtec high speed cable to connect QSPI from another board.

So I am planning to bidirectional buffer for QSPI, but not avilable any bi direction buffer for QSPI.  So I am using the TXB0106 bidirectional level translator with both VCCA & VCCB is 1.8V.

Will it work ? Is there any other solution for bi directional buffer which can use our design for QSPI?

Regards,

P. Rajkumar Kannan.