Other Parts Discussed in Thread: SN74LV4046A, , SN74LV393A
I'm trying to wrap my head around the usage of the aforementioned integrated circuit. I'm aware of how a PLL generally works but as the datasheet of this IC is the only source of information I have, I'm a bit lost how to integrate it into my circuit.
I need the PLL to generate a frequency that is 256 times higher than the input frequency which is a clean 50% square wave at around 80kHz - so, the output frequency is at ~20.5 MHz . The frequency division is taken care of using a counter IC. As I understand PLLs in general, the input signal (80kHz) must be applied to φA1, the output of the frequency divider is fed back to φB and the input to the divider is my output frequency (at 20.5MHz), when the PLL is locked. Input φB is also at 80kHz in this case.
But this digital PLL has a lot more pins that have to be some kind of filter and a controllable oscillator in a form that isn't obvious to me. Where does that leave the Mfc input and the I/D in/out, the modulo controls and so on? What frequencies are we talking about on those inputs and outputs for my usage scenario? The datasheet seems to have math as an answer to that question but I'm certainly not a math type of guy so some kind of usage instructions or even an example schematic diagram would be very helpful. Does it need more external components than the frequency divider?
Thanks!
Thomas