This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0102-Q1: Size of pull up resistors

Part Number: LSF0102-Q1


My customer used LSF0102-Q1 as a level shift.

Vref_A = 3.3V, Vref_B = 5V

They have some questions about using pull resistors.

1. Is it ok using 33kΩ as pull up resistor to  B side for customer's IC requirement?

2. Is it possible using 10kΩ as pull up resistor to A side to decrease current consumption?(Is it ok not to use pull up resistors by applying table in LSF0102-Q1 datasheet 9.2.1.2.2?)

3. Does LSF0102-Q1 operate well using pull up resistor to Vref_B pin not 200 kΩ but 100 kΩ?

Thank you.

Best Regards,

Kevin Shin