This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4504B: What's the default output level when VCC is not powered and VDD is powered?

Part Number: CD4504B
Other Parts Discussed in Thread: TLV760

Hi team,

My customer is using CD4504B to convert a 3.3V input to 15V output. During the whole system is powered up, we found that VDD is powered up earlier than VCC. So there's a short period that VDD is present and VCC is absent. And we captured a logic high output during this short period and this is not accepted by csutomer because they want a stable logic low output during the power up process

So I just want to check what's the default output level when VCC is not powered and VDD is powered? Is there any method we can use to keep the output low during power up? This device doesn't have a OE pin and it seems have a Push-Pull output structure so adding a pull-down resistor at the output may not help. So please help on this. Thanks.

Best regards,

Wayne

  • When the input side is unpowered, the signal seen by the output side is undefined.

    The simplest solution might be to power VCC from VDD with a small regulator (e.g., TLV760‍33), and to put a pull-down resistor at the input.