Other Parts Discussed in Thread: SN74LVC1G175, TLV809E, SN74LVC1G98
Hello,
Here is my set-up before powering up :
- Vcc and D input are tied together (in 3.3V level)
- LE signal cames from another part (in 3.3V level) and is set-up to 0 (gnd)
- /OE is tied to ground
When i put the power on (Vcc going from 0 to 3.3V), the Q output switch to 1 but i was expecting this output to remain at 0 as LE signal is still at 0. But this is not the case in reality.
Here a view of the electronic set up.
Thank you for helping me to solve this problem