This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC32373A: SN74LVC32373AZKER Substrate CTE Young's modulus

Part Number: SN74LVC32373A

Dear Sir or Madame.

I have got a question from a Customer who asking for CTE and Young's modulus SN74LVC32373AZKER substrate listed below..

I wonder if you can help me with this information please?

Thank you in advance!

Yours faithfully,

Mathias Axelssson

CTE and Young´s modulus for substrate material (according to material declaration it is “epoxy” with a proprietary filler, and plated copper).

 

Excerpt from material declaration:

 

- <HomogeneousMaterial name="Substrate">

<Amount unitOfMeasure="mg" weight="12.730000" />

- <SubstanceCatagory jigLevel="Supplier" name="Copper and Its Alloys">

- <Substance cas="7440-50-8" name="Copper">

<Amount ppm="522000" unitOfMeasure="mg" weight="6.645060" />

</Substance>

</SubstanceCatagory>

+ <SubstanceCatagory jigLevel="B" name="Nickel and Its Alloys">

- <Substance cas="7440-02-0" name="Nickel">

<Amount ppm="10700" unitOfMeasure="mg" weight="0.136211" />

</Substance>

</SubstanceCatagory>

- <SubstanceCatagory jigLevel="Supplier" name="Not Categorized">

- <Substance cas="" name="Proprietary Filler">

<Amount ppm="36000" unitOfMeasure="mg" weight="0.458280" />

</Substance>

</SubstanceCatagory>

+ <SubstanceCatagory jigLevel="Supplier" name="Other Nonferrous Metals and Alloys">

- <Substance cas="7440-47-3" name="Chromium">

<Amount ppm="300" unitOfMeasure="mg" weight="0.003819" />

</Substance>

</SubstanceCatagory>

+ <SubstanceCatagory jigLevel="Supplier" name="Other Nonferrous Metals and Alloys">

- <Substance cas="7440-31-5" name="Tin">

<Amount ppm="200" unitOfMeasure="mg" weight="0.002546" />

</Substance>

</SubstanceCatagory>

+ <SubstanceCatagory jigLevel="Supplier" name="Precious Metals">

- <Substance cas="7440-57-5" name="Gold">

<Amount ppm="9200" unitOfMeasure="mg" weight="0.117116" />

</Substance>

</SubstanceCatagory>

- <SubstanceCatagory jigLevel="Supplier" name="Thermoplastics">

- <Substance cas="85954-11-6" name="Epoxy">

<Amount ppm="421500" unitOfMeasure="mg" weight="5.365695" />

</Substance>

</SubstanceCatagory>

+ <SubstanceCatagory jigLevel="Supplier" name="Zinc and Its Alloys">

- <Substance cas="7440-66-6" name="Zinc">

<Amount ppm="100" unitOfMeasure="mg" weight="0.001273" />

</Substance>

</SubstanceCatagory>

</HomogeneousMaterial>”