This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC14A: Can Vcc of SN74LVC14A accept 5V?

Part Number: SN74LVC14A


Customer found they were using 5V as the power supply for SN74LVC14A.  In the datasheet, the absolute maximum voltage is 6.5V, but the recommended max VCC is 3.6V.  Could you please help check the risk for it? They also used these design in former projects, and now the new project is going to mass production. Thank you.