Other Parts Discussed in Thread: TXS0104E, , LSF0204
Hello Team,
We are using TXB0304RUTR level shifter for driving PCIe CLKREQ# signal which connected to PCIe based WLAN module. In module pin is defined as open drain, and suggesting to add pulled up at host side.
Below is our implementation in schematic.
While powering on we are not getting any activity on any side of level shifter for PCIE0_QCA_WL_CLK_REQ_N and due to that link initialization of PCIe is failed. We have checked enable voltage is coming high so seems no issue of enabling level shifter. Even though we have added 10k pulled up on Side A signal, still behavior remains same.
During further debugging, we have replaced TXB0304RUTR level shifter by TXS0101YZPR and WLAN we can see transition on PCIE0_QCA_WL_CLK_REQ_N line and able to do link initialization.
   
Can you please help us:
1) What is the major difference between TXB0304RUTR & TXS0101YZPR Level shifter?
2) Is there any timing difference for TXB0304RUTR which can cause issue for CLKREQ# line?
3) What can be other cause for TXB0304RUTR for above mentioned issue?
4) To eliminate HW change and PCB Re-spin, can you please help how we can drive signal with TXB0304RU?
Your Prompt reply is highly appreciated.
Regards,
Nimesh