Part Number: SN74AXC4T245
Hi,
Regarding the SN74AXC4T245 - can I assume that if the part is not powered from both sides - the input and output signals are high-z?
Thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AXC4T245
Hi,
Regarding the SN74AXC4T245 - can I assume that if the part is not powered from both sides - the input and output signals are high-z?
Thank you,
Thank you Clemens!
Hello Efi,
Clemens is correct, and the key here is that one of the supplies is actually connected and in a known state below 100mV.
If both supplies are "floating" then there is a chance that some charge could couple onto the line, causing the device to be enabled, in which case some of the ports may no longer be in Hi-Z.
Its a matter of making sure that the ports are at a known voltage.
Best,
Michael