This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Choice of level translator

Other Parts Discussed in Thread: SN74LVC1T45, SN74AVC1T45

Hi,

I would like to use an MSP430 mcu with a 3v Supply,

This needs to interface with a transciever which provides 3.3V digital output, using UART 

Even though the absolute rating in the MSP data sheet says, the input on the pins can go upto Vcc+0.3 V, it would be better not to stress the mcu.

Could anyone suggest a suitable level converter from 3.3V to 3V level.. or would be better to use Schottky diodes to drop the voltage?

Thanks,

Karthika