Part Number: CD40109B
I need clarification regarding CD40109B for following setting
Vcc=3.3V
ABCD= VIh 3.3V
Vdd= 15V
Enable=3.3V
Please confirm level shifting possible from 3.3V to 15V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD40109B
I need clarification regarding CD40109B for following setting
Vcc=3.3V
ABCD= VIh 3.3V
Vdd= 15V
Enable=3.3V
Please confirm level shifting possible from 3.3V to 15V
Thanks for the confirmation.
However this doubt I got because in the datasheet for only Vdd 3V-18V recommend operating voltage mentioned. For VIL max and VIH min range for my setting also not mentioned. Datasheet shows value for Vcc 5V/10V and corresponding VIL, VIH.
Both VCC and VDD are inside the recommended operating conditions.
VIL and VIH are not specified for 3.3 V, but signals near 0 V or 3.3 V are certain to be OK.