This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCH8T245: Delay time calculation

Part Number: SN74LVCH8T245
Other Parts Discussed in Thread: SN74LVCH16T245

Hi,

I have a doubt in estimating the maximum propagation delay for SN74LVCH8T245 when changing the DIR signal. For ex: My Vcca=5V & Vccb=3.3V. Initial data flow direction is from A to B (DIR=HIGH). If I change the DIR to LOW, how much time it would take to reflect the B side signals at A side?

Datasheet specifies,

I have two questions here.

1) I'm not sure which equation should I consider? Is it 1 or 2 or both.

2) We see a time delay to disable B port (tpLz/tpHz) & normal signal propagation delay (tpLH/tpHL). Should there be a time delay to enable the A port or is it already enabled?

Also datasheet spec says,

3) If tpzH (or) tpzL is the total delay from the moment we change the DIR signal & to get output signal at desired side (as per first screenshot), why tphZ/tpLz (~8ns) is specified more than tpzH /tpzL (~6ns). Please help me to have a correct understanding.

Thanks & Regards

Muthu A