This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: functional issue with 8-Channel TXB0108 device

Part Number: TXB0108
Other Parts Discussed in Thread: TXS0102

Dear Sir,

              I am using 8-Channel TXB0108 device in my circuit. The input is given from a USB-4751 module which is a 8 channel TTL INPUT/output device. I configuring it to output. the 5 v output is connected to B side and b side is at 5v supply. At side the supply is 3.3V and i am monitoring the output. when i switch the output from module to high and low some time the output(A side) remains at 3.3v and some times at 1.7v and some time it goes to 0vdc. I see the output is connected to input back. Do i need to take any precautions in design. Pleae help.

Thanks

Sanjay Parelkar