Other Parts Discussed in Thread: TXS0102
Dear Sir,
We are choosing a solution between TXB0102 and TXS0102. In our application is on the MDIO bus for interfacing devices at different interface voltages.
From the datasheet, we see that TXB0102 has a limitation, it can NOT be used in I2C or 1-wire that an open-drain driver is connected to the bidirectional data I/O. I'm not sure if TXB0102 can be used on the MDIO bus.
The circuits of TXB0102 and TXS0102 are shown below, and all details have been designed according to the datasheet. Please help to check if there are any problems.
TXB0102
TXS0102
Note.
1. VCCA (2.7V) ramps up first and then VCCB (2.85V) ramps up after ~12 sec.
2. The I/O drive strength at least 16 mA in our platform.