This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN54LVTH16244A: Internal ESD Protection

Part Number: SN54LVTH16244A

Team,

Can you share information about the internal ESD protection on the SN54LVTH16244A?

I need to design a protection circuit that interfaces with this buffer against a 4kV ESD transient following the Human Body Model. Current part is rated for 2kV HBM ESD which is not enough against 4kV. If information about the ESD protection circuit on this IC cannot be shared, then information about the type of diode (Silicon, Schottky, Zener) or breakdown voltage would help.

Let me know if there is a recommended way of designing an external ESD protection circuit that interfaces with this buffer (like an application note).

Thank you.