Part Number: SN74LVC125A
Other Parts Discussed in Thread: TXB0108
Hi Team,
I would like to buffer jtag signals (12mhz max) from an external connector to/from my board. The voltage is 3.3v.
I was looking at the SN74LVC125APWT , it seems a good choice , however its ESD HBM rating is quite low. I need to withstand 15kv.
I was looking also at the TXB0108, I could connect VCCA&VCCB to the same 3.3v, it has ESD rating of 15kv on the B port, however the output drive capabilities are low so i am not sure it is a good choise for jtag (signals have to exit my board for some distance....)
Beat Regards,
Tom Liu