Part Number: LSF0101
Other Parts Discussed in Thread: SN74LVC2T45, SN75LVDS387, SN75LVDS386, SN74LVC8T245
Hello TI team,
When I read the datasheet of the LSF0101, it seems that the current flowing to the I/O should be of the mA level (there are example for choosing pull-up resistor for 15mA, 10mA or 3mA and the test conditions are presented with current from 10mA to 64mA).
I need to use this translator for SPI communication. However, in the MCU I'm using, the SPI communication port have pull-up/down resistor of about 13kOhms. That means that for 5V there would be a current of approximately 385µA flowing in the switch of the LSF0101.
Would it still be alright or is there a minimum current value that should be flowing in the LSF0101 to make it work properly?
Thanks for your help.