This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: Input Current value

Part Number: TXB0108

Dear TI Team

We are considering voltage level conversion from 3.3V to 2.8V from B side to A side in the following form.


At this time, if there is data on the current value (current value drawn into the device) that is input to the B side when the voltage levels on the A side and B side are Low, please tell me.
(The data sheet only shows the input current value of the OE pin.)
Even if there is no current data for the above conditions, please let me know if there is a reference value when the input/output is low.

Best Regards,

Y.Ottey