Part Number: SN74HCT138
The datasheet said "+-4mA output drive at 5V" at page 1. At the page 3, the continuous output current , Io (Vo=0to Vcc) is +-25mA. What is the drain/source driving current at regular temperature (0-85 C)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74HCT138
The datasheet said "+-4mA output drive at 5V" at page 1. At the page 3, the continuous output current , Io (Vo=0to Vcc) is +-25mA. What is the drain/source driving current at regular temperature (0-85 C)?
Hey Daniel,
4 mA is the recommended max drain source current over the recommended operating temp (-40 to 85 C).