This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT541: Supply current and dissipation calculation

Part Number: SN74AHCT541


Hello,

I see that Figure 5 on the datasheet shows 270mA @50MHz 3.3V operation. ((270e-3/8)/50e6)/3.3 = 204pF per channel. Why is the current in that figure this high? I see in section 7.9 the power dissipation capacitance per buffer as 33pF. So I'd expect 8*33pF*3.3V*50MHz = 43mA total supply current instead of 270mA.

Kind regards,

Zeki