Part Number: SN74LVC1G07-Q1
Other Parts Discussed in Thread: SN74LVC3G07-Q1, SN74AVCH8T245, SN74AVC8T245
Hi experts,
We have a customer that is looking for 10-15mA source/sink at 1.8V. I see lots of buffers that support the 1.8V level but the max current is in the 4-8mA range.
Is there any high current, low voltage digital buffers?
If no, could I connect TWO inputs and outputs of a buffer to double the current?
THanks,
Connie