Other Parts Discussed in Thread: CD40109B, LM6511, LM311
Hi,
We have to level shift 15V to 5V, which is input to gate driver. So,can you suggest TI parts with low propogational delay for the same.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What do you mean with "low"?
The only logic devices for voltages above 5 V are in the CD4000 family. The CD40109B can be used as a high-to-low shifter, with a propagation delay of at most 500 ns at 25 °C.
Comparators like the LM6511 or LM311 are faster.