Part Number: TXB0104
Other Parts Discussed in Thread: SN74LVC125A
Hi,
We need to shift a bunch of 3V signals to 1.8V.
We first chose to use the TXB family to do, but the component connected to the low power side (VCCA) has internal pull-ups ont its IO line.
The internal pullups are 11k resistors, which are below the 50k recommended limit.
Would the TXB work in this condition? If not, how could I fix the issue?
Regards
Giuliano