This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G14: Can I replace SN74LV14AD with SN74LVC1G14DBVT ?

Part Number: SN74LVC1G14


Hello Team TI,

                        My application involves operating at 3.3V supply, in the old design we used SN74LV14AD (Hex Schmitt Inverter) as per application only one gate is utilized and rest of the 5 gates are left idle, is the product SN74LVC1G14DBVT (Single Schmitt Inverter)  compatible to replace SN74LV14AD, in our application the gate input is with an pull-up resistor and output is given to FPGA working at 3.3V.

Kindly Suggest

S.Sitarama Swamy