Part Number: SN74LV14A
Hi Team,
There are two definition of Vo abs max level in the datasheet as below.
It looks like we have to be careful about the relationship between the Vcc and Vout voltages when the Output is NOT Hi-Z, but what are the conditions under which Vout is Hi-Z?
Also, Can we regard as Vcc=0.3V condition is Power Off state?
Regards,
Takashi Onawa