This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AC241: Thermal resistance, junction to case? Or max junction temperature?

Part Number: SN74AC241


Looking at SN74AC241DW, there is only a theta_ja listed and an operating temp -40 to 85C. Is there a recommended max operating junction temperature and/or a corresponding theta_jc for this part?

Thanks,
Lauren

  • Hi Lauren,

    The max operating junction temperature is 150C -- see [FAQ] What is the maximum junction temperature (TJMAX) for a device?

    We have a much more accurate mathematical model for thermals now than when this part was originally developed (you may notice that all parts in a package used to have the same R_theta_ja).  These are the updated numbers for this device:

    Result- Theta JA-High K (standard datasheet value)

    81.4

    Result-Theta JC, top (standard datasheet value)

    46.8

    Result-Theta JB (standard datasheet value)

    49.3

    Result- Psi JT (standard datasheet value)

    20.0

    Result- Psi JB (standard datasheet value)

    48.8